(Interactive Access) Processes
This section shows a list including all the ongoing processes. They can be stopped by clicking the
End Processes
button.FactoryTalk Remote Access Manager
provides a Processes Manager
to assist in identifying running processes on remote devices, CPU usage percentage and memory usage.To access
Processes Manager
, proceed as follows:- Make sure that theFactoryTalk Remote Access Manageris connected to the remote device.
- Access.NOTE: TheProcessesfeature cannot be accessed throughInteractive Access (Web only).
- TheEnd processesbutton activates.NOTE: Use theEnd processesbutton to end any process, as needed.
Provide Feedback