Failed to reset alarm

Failed to reset alarm

Problem attempting to reset the alarm, indicating one of these conditions:
Reset not required for this alarm
Cannot reset an alarm that cannot be latched. Check
Latched
in the
Configuration
dialog box to enable latching for this alarm.
This alarm has already been reset
Cannot reset an alarm that was already reset.
Reset with wrong parameters
Invalid parameters were sent with the reset command.
Alarm input is still active
Cannot reset an alarm while the alarm input is still active. For example, if the alarm is triggered when condition = 0 and the current alarm input is 0, cannot reset the alarm.
Check the configuration, make necessary modifications, and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal