Confirm controller type change
After selecting
Change Type
in the Change Controller
dialog box, confirm to change the controller type. Carefully read the consequences of the change that are listed on this screen. Then select
Yes
to continue with the change or No
to keep using the existing controller.Provide Feedback