Advanced tab

Use the
Advanced tab
to view and edit the advanced controller properties.
TIP:
The parameters
System Overhead Time Slice
and
During unused System Overhead Time Slice
are not needed by controllers supported by versions 25.00.00 and later of the
Logix Designer
application, and have been removed.
TIP: To open the Advanced tab:
  1. In the
    Controller Organizer
    , expand the
    I/O Configuration
    folder, and double-click the controller.
  2. On the
    Controller Properties
    dialog box, click the
    Advanced
    tab.
Parameter
Description
Controller Fault Handler
This program runs when there is a system fault. Valid values include all unscheduled programs.
Power-Up Handler
This program runs when the processor powers up in Run mode after a power-down in Run mode. Valid values include all unscheduled programs.
Match Project to Controller
The
Logix Designer
application verifies that the serial number configured for the project matches the serial number of the controller when going online, downloading, and uploading. Verification does not occur when transferring a project from nonvolatile memory to the controller.
Match Project to Controller
is only enabled for controllers that support serial numbers.
Serial Number
The serial number of the controller to which this program is associated.
Serial Number
is only enabled when
Match Project to Controller
is selected.
Allow Consumed Tags to Use RPI Provided by Producer
Connects the consumed tags in the controller to the producer when the producer provides the Requested Packet Interval (RPI).
If the RPI of the consumed tag is outside the RPI range of the producer, the connection fails.
Allow Consumed Tags to Use RPI Provided by Producer
is only enabled when the controller is offline.
Report Overflow Faults
Reports minor Overflow faults.
Report Overflow Faults
is only enabled when the controller is offline.
The value of this check box is persisted in .ACD, .L5K, and .L5X files and downloaded to the controller. When the value is changed offline, the correlation between the
Logix Designer
application and the controller is broken. A full download or upload is required to reconnect to the controller.
IMPORTANT:
Selecting
Report Overflow Faults
may increase application scan time.
NOTE:
Selecting or clearing
Report Overflow Faults
changes the Safety Instruction Signature ID for Safety Add-On Instructions that include math instructions.
Enable Automatic Diagnostics
Automatically sends device diagnostic condition updates to applications and client devices supported by
FactoryTalk Alarms and Events
.
NOTE:
Supported only on
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580,
Compact GuardLogix
5380, and
GuardLogix
5580 controllers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.