- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Controller Properties dialog box - Minor Faults tab settings
The settings on the
Minor Faults
tab of the Controller Properties
dialog box display minor fault information that occurs in the controller and fault bits that have a specific fault type assigned to them.
The ability to change the settings on this tab can be controlled by
FactoryTalk Security
permissions.
IMPORTANT:
If selecting a
Fault Bits
check box that is not set, it writes to the controller and turns on the corresponding bit in the MinorFaultBits attribute in the FaultLog object. This gives a false indication that a minor fault is logged.Parameter | Description |
---|---|
Number of Minor Faults Since Last Cleared | Displays the number of minor fault events reported since the log was last cleared. |
Recent Faults | Displays a description of the last eight minor faults that occurred. These faults are stored in reverse chronological order. When offline, this field contains the stored contents of the last online session. |
Clear Minors | Clears the Minor Fault log. |
Fault Bits | Lists the minor fault bits that have a specific fault type assigned to them. If the bit is set, the check box is selected. These check boxes are not filters; they correspond to the MinorFaultBits attribute in the FaultLog object. When offline, these check boxes are unavailable, but display the contents of the last online session.
TIP:
The fault bit for backup energy depends on the device the controller uses to save the project upon power loss. The fault bit is either:
|
Provide Feedback