Controller Properties dialog box - PlantPAx tab
The
Controller Properties
dialog box displays controller configuration information for the open project and, when online, for the attached controller. The PlantPAx
tab displays information about PlantPAx controllers. Select options that control these PlantPAx properties:- Use PlantPAx Tasking Model.
- Instruction UsageTIP:ThePlantPAxtab is available only for PlantPAx controllers.
TIP:
To open the Controller Properties dialog box - PlantPAx tab:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click thePlantPAxtab.
Provide Feedback