Add a disconnected transition
Adding a disconnected transition (not connected to a step) is useful to:
- Replace an existing transition.
- Add a transition to a structure where an additional transition is needed, such as the first element in each branch of a selective divergence.
To add a disconnected transition:
- Select in the Sequence Editor workspace, or select on an element to connect to in the sequence diagram.
- On theEquipment SequenceElement toolbar, selectAdd Step and Transition Pair
.
- (optional) Right-click the existing link and then clickDeleteto remove any existing links from the element connectors.
- Click the connector of the first element to create a link, and then click the connector of the second element to attach the link.
Provide Feedback