Command a step or Equipment Phase using the Equipment Sequence Monitor

Command a step or Equipment Phase using the Equipment Sequence Monitor

Command an
Equipment Phase
through a step using the
Equipment Sequence
Monitor.
Before you begin:
  • Go online with the controller.
  • In the
    Equipment Sequence
    Monitor, open an
    Equipment Sequence
    .
  • The
    Equipment Sequence
    must be in
    Manual
    mode.
  • The step to be commanded must be active. This implies the step is attached to the
    Equipment Phase
    to be commanded. Select
    Active Step Change
    L5K_SILC_initializetags_icon_V25 to make a step active.
To command a step using the
Equipment Sequence
Monitor:
  1. Select
    Take Ownership
    to take ownership of the
    Equipment Sequence
  2. Select the active step to see the
    Equipment Sequence
    step command toolbar.
  3. Select a command to command the equipment phase associated with the step.
  4. (Optional) Once you have completed commanding phases, select
    Exit Manual
    to go back to
    Automatic
    mode.
  5. Select
    Release Ownership
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal