Configure Equipment Sequence properties
Configure dialog box.
Equipment Sequence
properties using the Configuration
tab in the Equipment Sequence
PropertiesBefore you begin:
- Go offline with the controller.
To configure
Equipment Sequence
properties:- Open theEquipment Sequence Propertiesdialog box by right-clicking the Equipment Sequence name in theController OrganizerorLogical Organizerand selectingProperties.
- Select theConfigurationtab and revise the properties as necessary.
- (Optional) Select theRetain sequence ID when resetting sequence option to retain the sequence ID when resetting the Equipment Sequence. If this option is not selected, a RESET command clears the Sequence ID value of an Equipment Sequence.
- (Optional) Select theGenerate sequence eventsoption to generate sequencing events recording the manufacturing process. This includes operator commands, changes in sequence attributes, and changes in sequencing parameters and step tag values.
- (Optional) When selecting theGenerate sequence eventsoption, enter a number for theUnit IDoption. TheUnit IDis an integer value assigned to represent the equipment unit the sequence is coordinating. This value is recorded with sequence events to identify the equipment coordinated.
- (Optional) When starting sequence, there are two options:
- Use initial value of the tag: Select this option to reinitialize all sequencing parameter and step tag value fields with their configuredInitial Valuefield when a START command is sent to theEquipment Sequence.
- Use current value of the tag: Select this option to retain the value of all sequencing parameter and step tag value fields when a START command is sent to theEquipment Sequence.
- (Optional) When resetting sequence, there are two options:
- Restore the tag to its initial value: Select this option to reinitialize all sequencing parameter and step tag value fields with their configuredInitial Valuefield when a RESET command is sent to the sequence.
- Maintain current value of the tag: Select this option to retain the value of all sequencing parameter and step tag value fields when a RESET command is sent to the sequence.
Select the 
Inhibit equipment sequence
check box to prevent the
controller from executing this Equipment Sequence
. Clear the check box and the
controller will execute the Equipment Sequence
. The check box is clear by
default. If the Equipment Sequence
is inhibited, n Equipment Sequence
icon
displays in the Controller Organizer
with the inhibited
decorator: 
Provide Feedback