- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Enter Module References in the Ladder Editor
Two types of module references display in the
Module Browser
:- TheParametersfolder at the top lists any Program InOut Parameters of the MODULE data type.
- TheI/O Configurationfolder lists the available modules.
To enter a module reference in the Ladder Editor
- In the instruction, chooseModulefor theClass Name.
- Perform one of these actions in the GSV or SSV instruction:
- Type the name for the program's module reference parameter or module intoInstance Name.
- Select the down arrowInstance Nameand choose a module reference parameter or module from the in-place Module Browser.
Provide Feedback