Routine Properties dialog box - General tab - Ladder Routine parameters

The
General
tab on the
Routine Properties
dialog box lists the properties associated with the selected function block routine. This table describes the parameters on the
General
tab.
Parameter
Description
Name
The routine name, which must use the
Logix Designer
application IEC-61131 Name Standard.
Description
A description for the routine that contains a maximum of 512 characters.
Type
The language type of the main logic in the routine: Ladder, Function Block Diagram, Sequential Function Chart, or Structured Text.
In Program
The program to which the routine belongs.
Class
Indicates whether the routine is a Standard routine or a Safety routine. This setting applies to Safety applications only.
Number of rungs
The number of rungs in the routine.
Permission Set
Applies a set of permissions that controls access based on the permissions configured in
FactoryTalk Security
. The default setting,
<Controller Inherited>
, applies the same security settings that have been applied to the controller or project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.