MotorOvertempFault

MotorOvertempFault

Applies to: Servo Drive axes.
MotorOvertempFault is a Boolean attribute. It is set when the motor’s temperature exceeds the motor shutdown temperature.
MotorOvertempFault is a recoverable condition.
To clear a MotorOvertempFault:
  1. Reduce motor loading and/or the ambient temperature.
  2. Be sure your program or fault handling routine contains either a:
    • Fault Reset (MAFR) instruction, to clear all motion faults for an axis, or
    • Shutdown Reset (MASR or MGSR) instruction to return to the axis ready operating state.
The occurrence of a MotorOvertempFault on a Servo Drive axis sets bit #18 of the DriveFault attribute, the PhysicalAxisFault attribute, and bit #0 of the AxisFault attribute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal