PNPOS time settings
Use the
Advanced > Time configuration
tab on the PNPOS Properties
dialog box to configure time parameters for Process n-Position Device (PNPOS) instructions.To configure time settings for PNPOS instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Enter values for the amount of time, in seconds, to delay feedback for each of the feedback types for loopback tests or for when the device feedback is not used:
- Time to reach target position
- Time to lock or unlock
- Time to index cylinder
- Enter values for these settings:
- Time to get lock feedback before fault. Number of seconds to allow for device lock or unlock feedback after a lock or unlock command. If the feedback is not received within this number of seconds, a Lock Failure status is triggered.
- Time to get position feedback before fault. Number of seconds to allow for device position feedback after a position command. If the feedback is not received within this number of seconds, a Position Failure status is triggered.
- Delay before extending cylinder to engage for move. Number of seconds to delay before extending the cylinder to engage for a move.
- Delay to verify device has settled in commanded position. Number of seconds to delay verifying that the device has settled in the commanded position.
- Number of retries via Position 1 before declaring failure (0=don't retry). Enter the number of retries before the move is considered a failure.
- Time to sound audible on commanded energize (0=disabled). Enter the number of seconds to sound an audible notification when the device is energized.
- SelectApply.
Provide Feedback