HMI navigation for PAI
Use the
HMI Navigation
tab of the PAI Properties
dialog box to enable or disable navigation from the HMI to the input and output PV objects for Process Analog Input (PAI) instructions.To enable HMI navigation to input and output objects for PAI instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- To allow navigation to the PV input, PV output, and smart device objects from the HMI faceplate, selectAllow navigation.
- In theObject tag namebox, enter the name of the object.NOTE: The name of the smart device object must match the name of the PAI object with_Dvcappended to the end of the tag name.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state, such asPV goodorPV uncertain.
- Device issues. Displays fault conditions, such asPV badorConfiguration error.
- SelectApply.
Provide Feedback