HMI navigation information for PHLS
Use the
HMI Navigation
tab of the PHLS Properties
dialog box to enter navigation information for the selected Process High or Low Selector (PHLS) instruction to label HMI faceplates.Enter HMI navigation information for PHLS instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select the arrow next toHMIand then selectHMI Navigation.
- Set the parameters:
- Allow navigation. Select to allow navigation to the input and output object from the HMI faceplate.
- Object tag name. Type the name of the object to navigate to if navigation is allowed. Text should contain the default controller path and default device. For example, /AREA::[SHORTCUT]Tag.
- View the read-only parameters:
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Off, Pulse on, or Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Feedback fault or I/O fault.
- SelectApply.
Provide Feedback