- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
HMI navigation for PLLS
Use the
HMI Navigation
tabs on the PLLS Properties
dialog box to configure navigation to individual motor faceplates in the motor group for up to 30 motors.To enable HMI navigation to motor faceplates for PLLS instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation 1-15orNavigation 16-30.
- To allow navigation to a motor faceplate from the HMI faceplate, selectAllow navigationfor each motor.
- In theObject tag namebox, enter the controller path, the device tag, and the motor number. For example, the object tag name for motor 5 could be /North_Area::[ProcessStrategies]MT05.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state:
- None
- Stopped
- Running
- Stopping
- Decreasing
- Increasing
- Device issues. Displays fault conditions:
- None
- Configuration error
- Fail to start
- Fail to stop
- SelectApply.
Provide Feedback