PPID loop settings
Use the
Loop mode
tab on the PPID Properties
dialog box to configure loop settings for Process Proportional + Integral + Derivative (PPID) instructions.To configure loop settings for PPID instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- UnderAdvanced, select theLoop modetab.
- Configure these settings:
- Allow auto loop mode. Enables Auto loop mode.
- Allow manual loop mode. Enables Manual loop mode.
- Allow cascade/ratio loop mode. Enables Cascade loop mode. Select the Cascade loop mode to us:
- Cascade. Selects regular Cascade loop mode.
- Ratio. Selects Cascade loop mode for Ratio.
- Go to manual loop mode on initialization. Sets the loop mode to manual when the PPID instruction is initialized.
- Lock in normal loop mode. Locks the loop in the mode configured as Normal.
- Normal loop mode. Select the Normal loop mode:Disabled,Manual,Auto, orCascade.
- PV fail response on. Select the conditions that trigger a PV fail status response on PV quality:
- PV bad
- PV bad or replaced
- PV bad, replaced, or uncertain
- Power up loop mode. Select the loop mode for power-up:
- Use the last loop mode applied
- Manual
- Auto
- Cascade
- Normal
- Power up CV value. Sets the CV value in CV engineering units to be applied during power-up. Use theHMItab to label the unit values.
- Power up SP value. Set the SP value in PV engineering units to be applied during power-up. Use theHMItab to label the unit values.
- When online with the controller, monitor theDevice state,Device issues, andDevice modeindicators at the bottom left of the dialog box:
- Device state. When theLogix Designerapplication is online with the controller, displays the current device state, suchSP rampingorCV held.
- Device issues. When theLogix Designerapplication is online with the controller, displays fault conditions, such asPV uncertain,SP fail, orConfiguration error.
- Device mode. When theLogix Designerapplication is online with the controller, displays the current device mode:
- Manual
- Auto
- Cascade (no Ratio)
- Ratio
- SelectApply.
Provide Feedback