HMI text for PVLV instructions

Use the
HMI
tab of the
PVLV Properties
dialog box to enter text that appears on HMI devices for Process Valve (PVLV) instructions.
To enter HMI text for PVLV instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Select the
    HMI
    tab.
  3. Configure these settings:
    • Library name
      . Associates instructions with a display library for faceplate call-up.
    • Instruction name
      . Associates the instruction name for faceplate call-up.
    • Display label
      . A label that appears on the graphic HMI symbol.
    • Area name for security
      . The area name for area-based security in the HMI.
    • Help button URL
      . URL for accessing help from the HMI.
    • Enable navigation to an object with more information
      . Select this checkbox to enable navigation to another source of information. In the box, enter the navigation path to the object, document, or website.
    • Operator command confirmation required
      . Configure operator commands and settings to require confirmation or to apply an e-signature from the HMI. Select:
      • None
        –command requests do not require confirmation by the operator.
      • Command confirmation
        –command requests require confirmation by the operator. This option displays a dialog asking the user to confirm the action.
      • Performer e-signature
        –command requests require an operator signature. This option enforces security from the HMI and disables commands and settings from the Logix Designer dialog.
      • Performer and approver e-signatures
        –command requests require both operator and supervisor signatures. This option enforces security from the HMI and disables commands and settings from the Logix Designer dialog.
  4. When online with the controller, monitor the
    Device state
    and
    Device issues
    indicators at the bottom left of the dialog box:
    • Device state
      . Displays the current valve state, such as
      Pulse continuously
      or
      Out of service
      .
    • Device issues
      . Displays fault conditions, such as
      Feedback fault
      or
      Transit stall
      .
  5. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.