Connect two steps in a sequence
To execute 1 or more steps in sequence they must be connected in the SFC.
To connect two steps in a sequence
- Click the second step in the series.
- Press theShiftkey and click the transition that is under that step.A selection box shows around the step and transition.
- Drag the pair until a green dot appears on the first transition.
- Release the pair.The lower step connects to the transition of the upper step. A selection box shows around the step and transition.
Provide Feedback