Create selected branches
Use selected branches to execute one path or skip one or more paths depending on logic conditions.
To create selected branches
- Click the step for the first branch.
- Press theShiftkey and click the transition that is under that step.
- Drag the step and transition to the location for the first branch.
- Drag the steps and transitions for the remaining branches.
- Add an initial transition for each branch and drag the transition to the start of a branch.A green dot shows a valid connection.
- To connect the branches, click the pins in the order shown in the following illustration.A green dot shows a valid connection point. (Pins E and F may already be connected.)
To end selected branches
- Connect the branches by clicking the pins in the order shown in this illustration.A green dot shows a valid connection point.Transitions are inside the horizontal lines.
Provide Feedback