Jump to a different step
Connect a step to a different point in the SFC to:
- Jump backward or forward to another step in the flowchart (for example, loop back and repeat steps).
- Return to the beginning of the SFC and start over.
For example:

![]() | If its condition is true... |
![]() | ...jump to this step |
To jump to a different step
- Click the lower pin of the transition that signals the jump.
- Click the top pin of the step to which you want to go.A green dot shows a valid connection point. Typically, the resulting connection orients itself along the center of the flowchart and is hard to see.
- To make the jump easier to read, drag its horizontal bar above the step to which the jump goes.
- For example, to go to Step_001 from Tran_003:Click here.Then click here.Drag the horizontal bar here.Green dot.
Provide Feedback