- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Add a common header to Structured Text routines
Use a common header to automatically add text to the beginning of new Structured Text routines.
To add a common header to Structured Text routines:
- ClickTools>Optionsto open theWorkstation Optionsdialog box.
- Click theStructured Text Editorcategory.
- To open a text box editor, selectInclude Header on Create.The text box is pre-populated with information blocks: <Company Information>, <Developer Name>, <Routine Name>, <Description>, and <Date>.The blocks are filled in automatically from the company name provided when theLogix Designerapplication is installed, the name of the user who created the routine, the routine name and description, and the current date. However, if you replace one of the information blocks with text that you type, that information block is not automatically updated. For example, if you replace <Routine Name> with Routine A, then Routine A appears in every header.You can also change the layout of the header, including the placement or order of the information blocks.
- ClickApplyto save the header text.
- ClickOKto apply the changes for new routines.
Provide Feedback