Language Element Toolbar

Language Element Toolbar

The Language Element toolbar is a tabbed toolbar, which shows the instruction set available for your language, as tabbed categories on the toolbar. When you click a category tab, the instruction toolbar just above changes to show that category of instructions.
This toolbar also has two scrollbars: one for the tabbed instruction groups, and one for the instructions within a group. Simply click these scrollbars to move through the groups or instructions. You can also resize this toolbar by dragging on its left or right edges.
Specialized toolbars are available for each language.
TIP: In Logix Designer versions 37 and later, the
Language Element
toolbar is hidden by default. To display it, select
View > Toolbars > Language element
. The Instruction Toolbox appears by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal