Loading
Blog
Recent ActivityRecent Activity
3 minute read

Water/Wastewater: Drive Out Distortion With a Low-Harmonic Drive

Drives with built-in distortion mitigation help protect process integrity and uptime in water/wastewater operations.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
people pouring tap water into large plastic bottles

Get Low: Reduce Harmonics in Water/Wastewater with In-Drive Technology

There’s a contaminant that has long troubled water and wastewater operations, and you won’t find it in the water.

Harmonic distortion is like a pollutant on a power line. It can cause electrical equipment to act erratically or shut off, resulting in unplanned downtime. And it can frustrate workers by making water treatment systems more difficult to optimize.

The IEEE 519 standard gives industry a target to achieve: a total harmonic distortion of 5% or less. The question is, how do you hit this target with minimal risk or impact to your operations?

The answer, it turns out, is mitigation technology in your drive.

A Contained Solution

A low-voltage AC drive with built-in harmonic mitigation offers several benefits compared to other mitigation solutions.

First and foremost, it can reduce the effects of harmonic distortion to help you comply with the IEEE 519 standard. But it also provides panel and floor savings compared to using external devices, like harmonic filters or 18-pulse transformers. And it reduces the wiring costs and installation time that can come with those devices.

An in-drive solution also puts the burden of managing the mitigation on the drive manufacturer.

This means if you work in water and wastewater operations, you don’t have to specify, install and maintain extra technology beyond the drive itself. It also means you don’t have to worry about the new technology impacting your drive’s performance – like the efficiency losses that can be caused by a transformer’s heat.

Inside an In-Drive Solution

Low-voltage AC drives with active front-end technology can prevent harmonic distortion detected inside the drive from impacting the broader electrical network.

A few key components in the drive help this happen. First, an LCL filter provides low-harmonic capability and minimizes the current distortion into the utility grid. Also, a line-side converter draws energy without harmonic distortion and converts it to DC power.

Of course, harmonic mitigation is only one of many benefits you get from these drives.

For example, the drive’s active front-end technology can also help cut your energy costs. It can provide regenerative capabilities, so you can put excess energy back onto the incoming power supply. And it can reduce fan speed and set the drive or bus supply in a low-energy state, which can reduce your energy consumption.

A drive that’s designed using an integrated architecture approach can also reduce your programming time and ease startup and commissioning. This design approach allows you to configure and program not only the drive but also your controller and other devices all in one development environment. It also allows you to use a single file for both your controller and drive configurations.

Reduced Harmonics, Reduced Hassle

A drive that reins in harmonic distortion to an acceptable level can help you avoid harmonics-related disruptions in water and wastewater treatment systems while realizing other savings. And because the mitigation solution is integrated into the drive, you don’t have to worry about how it will affect your footprint, installation demands or overall performance.

Learn more about low-voltage AC drives that use active front-end technology here.

Published August 9, 2019

Topics: Optimize Production Water Wastewater

Kelvin Hurdle
Kelvin Hurdle
North America Water Wastewater Industry Manager, Rockwell Automation
With 20+ years at Rockwell Automation in a variety of industrial automation roles, Kelvin Hurdle has an expansive knowledge of automation and process control. He is currently a company authority on Water/Wastewater applications, resulting from 30+ years of involvement in the industrial and municipal water industry.
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
How Advanced Automation Accelerates Industrial Adoption of SMR Technology
How Advanced Automation Accelerates Industrial Adoption of SMR Technology
Blog
Blog
How Advanced Automation Accelerates Industrial Adoption of SMR Technology
Rockwell Automation has the expertise, experience and partners to help make small modular reactors a viable energy solution for your facility.
Five Scaling Challenges Facing Colo Data Center Providers
Five Scaling Challenges Facing Colo Data Center Providers
Blog
Blog
Five Scaling Challenges Facing Colo Data Center Providers
Discover how Rockwell Automation helps colocation data center providers address key challenges, and scale with agility, security, and speed.
Sustainability as Strategy
Sustainability as Strategy
Blog
Blog
Sustainability as Strategy
How Rockwell Automation Is Redefining Industrial Sustainability Leadership Through the World Economic Forum
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left Water/Wastewater: Drive Out Distortion With a Low-Harmonic Drive Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose