Loading
Case Study | Mining
Recent ActivityRecent Activity
2 minute read

Actualizing Sustainability with Energy Drive

Energy Drive Uses Variable Speed Drive Technology to Help Clients Achieve Sustainability Targets

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
sibayne stillwater mine site in south africa

Meet James Hynd, CEO of Energy Drive

. The firm partners with companies from a range of energy-intensive industries to actualize energy-related sustainability goals.

“Ultimately what we do is deliver energy savings and with that we deliver carbon reduction,” James says. “If you think about our offering, it’s supporting and partnering around delivering sustainability for clients to achieve their targets. It’s the right thing to do and for that to be achieved at not just low cost, but at a net savings is quite significant.”

Watch the Video

Video Player
Chevron DownChevron Down
Energy Drive Actualizes Sustainability
Download File

Media error: Format(s) not supported or source(s) not found

Download File: https://rockwellautomation.scene7.com/is/content/rockwellautomation/energy-drive-actualizes-sustainability-en
00:00
00:00
00:00
Use Up/Down Arrow keys to increase or decrease volume.
Video
Actualizing Sustainability with Energy Drive

Energy Drive Uses Variable Speed Drive Technology to Help Clients Achieve Sustainability Targets

James Hynd, CEO, Energy Drive

James HyndCEO, Energy Drive

Improving Energy Efficiency

Sibanye-Stillwater

, a multinational mining and metals processor, engaged Energy Drive to improve and accelerate the energy efficiency of their mine ventilation systems. Energy Drive focused first on the large surface ventilation fans used in two of Sibanye’s gold mines in South Africa. Ventilation in underground mining is critical but uses a lot of energy.

“Due to health and safety, there’s always at least one fan fully operational and another in standby in case there’s a failure,” James explains. “We installed and optimized VFDs (variable-frequency drives) on the motors of both fans and then turned (the speeds of) them down while running them together.”

Significant Sustainability Benefits

Using Rockwell Automation PowerFlex® 6000T

VFDs to control and reduce the fan speeds, Energy Drive delivered an average of 62% in energy savings in the first shaft and 48% in the second. The two upgraded shafts have been operational for nearly a year, and they’ll soon commission a third shaft. James projects the three upgrades will deliver an energy savings of about 360 gigawatts (GWh) over the term of the contract.

That’s equal to removing, “5000 homes in South Africa from the grid every month. More importantly, measuring on actualizing sustainability, it will save 379,000 tons of carbon over the period,” James adds. The optimized systems have also significantly reduced water and coal consumption.

Helping Protect Miner Safety

Best of all, Energy Drive electronically controls the upgraded systems from the surface. “All of our systems are monitored 24/7 with pre-set alerts on key conditions,” James says. “Now that we’re running both (fans), if one fails our system automatically ramps up the other so that we never ever put the health and safety of the miners underground at risk.”

Another benefit of monitoring and running both fans is improved equipment performance and maintenance.

James credits the project’s overall success to an “extremely collaborative” client “committed to using technology to improve operational performance and safety, and Rockwell Automation’s technological excellence.”

Read more about how Energy Drive, Rockwell Automation and Sibanye-Stillwater collaborated

to realize significant energy savings and find additional project details here
.  

Published January 30, 2023

Topics: Drive Sustainability Mining Motor Control Centers, Low Voltage Motor Control, Medium Voltage Low Voltage AC Drives Medium Voltage AC Drives Drives
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
Drillmec optimizes carbon-capture operations through deployment of precision drive solution
Drillmec optimizes carbon-capture operations through deployment of precision drive solution
Case Study
Case Study
Drillmec optimizes carbon-capture operations through deployment of precision drive solution
Drillmec is an international leader in design, manufacturing, and distribution of drilling and workover rigs for onshore and offshore applications as well as a wide range of drilling equipment.
Solid Foundation for Expansion-Driven Digital Transformation
Solid Foundation for Expansion-Driven Digital Transformation
Case Study
Case Study
Solid Foundation for Expansion-Driven Digital Transformation
Probiotical S.p.A. maintains and improves manufacturing metrics, while scaling its operations, thanks to FactoryTalk InnovationSuite solutions
Pharbaco Sets New Standard for Smart Pharmaceutical Manufacturing
Pharbaco Sets New Standard for Smart Pharmaceutical Manufacturing
Case Study
Case Study
Pharbaco Sets New Standard for Smart Pharmaceutical Manufacturing
Leading pharmaceutical manufacturer achieves GMP-EU compliance with advanced automation and energy-efficient cleanroom solutions.
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right
  5. Chevron LeftChevron Left Actualizing Sustainability with Energy Drive Chevron RightChevron Right