Loading
Case Study | Mining
Recent ActivityRecent Activity
3 minute read

ReThink Milling Innovates Toward Zero-waste Mining

In a first of its kind venture, ReThink Milling unites over a dozen mining industry leaders in shared research & development to drive sustainability.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
mining grinding equipment ball mills in series
 

Gillian Holcraft is an innovation manager with the Canadian Mining Innovation Council

(CMIC). The consortium of operators and innovators was formed to reduce the mining industry’s environmental footprint by 50% by 2027 with a focus on energy, water and waste.

Mining consumes up to 6% of the world’s energy with 50% used to grind material into smaller particles, a process called comminution. Yet, it’s been more than two decades since the last advance in grinding equipment. That’s about to change as CMIC members are on a quest to ReThink Mining.

Watch the Video

 
Video Player
Chevron DownChevron Down
CMIC Innovates Toward Zero-waste Mining
Download File

Media error: Format(s) not supported or source(s) not found

Download File: https://rockwellautomation.scene7.com/is/content/rockwellautomation/cmic-innovates-zero-waste-mining
00:00
00:00
00:00
Use Up/Down Arrow keys to increase or decrease volume.
VIDEO
ReThink Milling Innovates Toward Zero-waste Mining

In a first of its kind venture, ReThink Milling unites over a dozen mining industry leaders in shared research & development to drive sustainability.

 
gillian holcroft president rethink milling inc

 

Gillian Holcraft

Innovation Manager at CMIC & CEO of ReThink Milling

Voice of Customer Drives Innovation

“The mining industry is known to be very conservative. We’re bringing the industry together to co-develop disruptive technology that could never be developed by a single company,” Gillian says. Council members provide “technology experts and insights. They’re telling us what the market wants to adopt something that’s completely new and different.”

Through the CMIC, the voice of the customer is driving industry innovation.

“When you’re working together as a team, innovation happens at the speed of trust,” Gillian says. “You talk about real issues and what it will take to bring in technology and actually end up using it.”

Revolutionary New Grinding Technology

The CMIC has several exciting projects underway including the development of the Conjugated Anvil Hammer Mill (CAHM) and MonoRoll Platform

. Together, these two machines have the potential to reduce energy consumption by 65% compared to the current comminution process. Another benefit is this revolutionary new technology will eliminate the need for secondary crushing mills, equipment and related transportation.

“Because we’re not using conventional steel balls as grinding media, we won’t have to produce and ship them. That’s a huge Scope 3 type of (carbon emission) reduction,” Gillian explains. “Not only are we going to reduce energy consumption, but we’ll ultimately simplify flow sheets and make the whole grinding process less costly.”

Data Collection Key to Commercialization

Initial machine testing has shown promising results for the patented CAHM and MonoRoll Platform. The project features several Rockwell Automation technologies including ControlLogix® programmable controllers

, PowerFlex® variable speed drives
, PanelView™ visualization software
, and FactoryTalk® Historian software
for data collection.

“We need to collect data to show not just that we can break rocks efficiently, but also how the machine is working so we can develop that next generation machine,” Gillian says. “Rockwell Automation’s technical team has been instrumental in helping us get the required data so we can build the next commercial unit.”

To commercialize and identify mine demonstration sites for the CAHM and MonoRoll Platform, the CMIC has formed ReThink Milling Inc. They hope to install and start CAHM demo testing in 2023 and secure the MonoRoll site in 2024.

Learn more about the work ReThink Milling

(whose members include over a dozen industry leaders, including Rockwell Automation) are doing to drive innovation in the mining industry here.

Published May 30, 2023

Topics: Sustainability Integrated Architecture Industrial Networks Mining ControlLogix FactoryTalk Historian Low Voltage AC Drives Drives Human Machine Interface Industrial Control Products Programmable Controllers Sensors & Switches Safety Products
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right
  5. Chevron LeftChevron Left ReThink Milling Innovates Toward Zero-waste Mining Chevron RightChevron Right