Medium-voltage drives offer sensorless vector control and new output-voltage ratings
MILWAUKEE — Users in heavy industries have a new motor control option for compressors, pumps and fans. Allen-Bradley PowerFlex 6000 medium-voltage AC drives from Rockwell Automation offer expanded, user-friendly control for variable and constant torque applications. The latest release delivers a wider voltage range (2.4 to 11 kV) and provides 100 percent starting torque, leveraging sensorless vector control.
The PowerFlex 6000 drive is easy to commission, use and maintain, with standard faceplates and EtherNet/IP connectivity. The drive is a cost-effective solution for heavy industries with higher power needs for their applications.
“Our scalable portfolio of medium-voltage drives offers a breadth of functionalities to best fit application needs,” said Brad Bugiardini, senior product specialist, Rockwell Automation. “Together with the PowerFlex 7000 drive, users can now select the right feature set for their application requirements.”
With an extended power range, the drive can be used for applications with output-voltage ratings up to 11 kV and motor current ratings up to 680 A, while remaining an air-cooled design. With eco-designed main cooling fans, users in Europe and other IEC-based markets can meet EC regulation 327 and ErP directive 2009, and avoid the larger footprint of a liquid-cooled drive. Internally powered cooling fans reduce customer-supplied control power requirements, and equipment and installation costs. A tertiary winding on the isolation transformer provides internal power for the fans.
![powerflex](https://s21.q4cdn.com/683968908/files/images/PR_images/2017/August/08-21-17-PowerFlex-6000-web.jpg)
Click to download image.
Two new output-voltage ratings are available – 6.9 kV for North America, and 11 kV for EMEA and Australia. The full range of ratings includes 2.4, 3, 3.3, 4.16, 6, 6.3, 6.6, 6.9, 10 and 11 kV.
With optional, automatic cell bypass up to 680 A, users can keep their operations running in case of a power cell failure and reduce unplanned downtime. In addition, an uninterruptible power supply helps increase system reliability, minimize downtime and mitigate potential machine damage.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Stephanie Winterhalter
Rockwell Automation
262.512.2369
sawinterhalter@ra.rockwell.com
Beatrice Zvosec
Padilla
612.455.1914
beatrice.zvosec@padillaco.com
Allen-Bradley and PowerFlex are trademarks of Rockwell Automation Inc.
EtherNet/IP is a trademark of ODVA Inc.
Published August 21, 2017