Program attributes
This table describes program attributes.
Attribute | Description |
---|---|
Name | The name of the program. |
Parameters | (optional) Input, output, or InOut parameters of the program. |
Properties | (optional) Properties of the program. |
Tags | Local tags contained within this program. |
Routines | Routines in this program. |
Provide Feedback