- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Configure idle Timeout
You can configure a timeout when there is a lack of user activity in the
FactoryTalk Optix Studio
application. A timeout can trigger any custom event. To configure a timeout, the application must have interactive graphic objects. At runtime, inactivity includes a lack of cursor movements, keyboard actions, and user interactions.
You can configure an idle timeout for either a specific page or an entire session.
Provide Feedback