Set dynamic variables polling time for controllers

Set dynamic variables polling time for controllers

Set the time interval between readings of tag values from controllers at runtime.
  1. In
    Project view
    , select
    NativePresentationEngine
    or
    WebPresentationEngine
    .
    For more information, see Presentation engines.
  2. In
    Properties
    , set
    Dynamic variables polling time
    .
    TIP: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal