- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Drawing tools
Use drawing tools to create custom objects to appear at runtime.
Use the drawing tools to draw free-form and one-dimensional objects including:
- Rectangles and squares
- Ovals and circles
- Lines
- Polylines and polygons
By default, each drawing object has a
MouseDown event
and MouseUp event
to which you can add methods.To prevent a drawing from snapping to the grid as you draw, in
, clear

Grid settings
Snap to grid
.Provide Feedback