- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Commit a library
Commit changes to a local or remote library to save changes on the local computer only. Committed changes are not backed up (or pushed) to a remote repository.
Prerequisites
- To commit a library
- From the main toolbar, select.Template Libraries
- SelectCommit.
- Enter a meaningful commit message.
- SelectOK.
A new version of the library is saved on the local computer.
Provide Feedback