Approve a remote connection from FactoryTalk Remote Access to a device

Approve a remote connection from FactoryTalk Remote Access to a device

If you are on a panel and
Approve Remote Access
is enabled in the
FactoryTalk Remote Access
application, you may receive requests from
FactoryTalk Remote Access
users who are trying to connect remotely to the device. You must then approve or deny a request to connect to the remote device.
  1. On the device, open the screen with the
    FactoryTalk Remote Access
    Widget.
    If you created your project using the OptixPanel template on the start page, select
    Settings
    and then select
    FT Remote Access
  2. Connections
    on the widget displays the
    FT Remote Access runtime version
    that is running on the device.
    A message appears at the bottom of the FT Remote Access widget to either approve or deny the request.
  3. To allow the
    FactoryTalk Remote Access
    user to connect to the remote device, select
    Yes
    to approve the connection, or select
    No
    to deny the request.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal