- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Duplicate a data logger
Duplicating a data logger configures a new logger based on the existing logger.
- From the toolbar, select.Open dashboard page
- In the editor, selectConfigure a data logger.
- Right-click the data logger to duplicate and selectDuplicate.A new data logger appears in the list of available data loggers.
Edit the duplicated logger settings. See Edit a data logger.
duplicate
Provide Feedback