- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a folder
Create a folder to contain nodes in your project.
You can create multiple versions of any folder. When you create a folder, the folder automatically has a context menu that you can right-click to create items specific to that folder category. Each folder category has an icon before it.
- InProject view, create either:
- Folder. Right-click the node to contain the folder and then select .
- Category folder. Right-click the project level node, selectNew, and then select the category of folder.
The
NewFolder#
appears in Project view
.folder
Provide Feedback