- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Paths
You can use path shortcuts when developing your application logic.
Shortcut | Description |
---|---|
%PROJECTDIR% | A directory that contains files transferred at runtime (images, documents, and so on). Example: C:\Users\ UserName \Documents\Rockwell Automation\FactoryTalk Optix\ ProjectName |
%APPLICATIONDIR% | A directory that contains objects used at runtime, including these objects:
|
%USB ,N %where N is a number associated with the USB device. | A path to a specific USB device connected to the target device. |
path
Provide Feedback