- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Variables
A variable is an attribute of an object. Assign a value to a variable to display the value at runtime.
View variables from either:
- Project view. Navigate to the folder containing the variables. TheUIfolder cannot contain variables.
- Properties. Select an object, type, or variable inProject viewor select and object in the editor. The variables or properties for the selected item appear inProperties.
attribute
value
Provide Feedback