- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Duplicate a project
Duplicate a project to use an existing project as a template for a new project.
- Open the project to be copied and then from the main menu, selectSave as.
- InSave project as, complete:
- Name. The name of the new project.
- Location. The storage location of the project files. The duplicated project is stored in the same location as the original project by default. Select the folder icon to browse to a new location.
- (optional)Use Version Control. Select to save your project in a Git repository.TIP: In order to use version control, FactoryTalk Optix project names and repository names must match. The project and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
- SelectOK.
duplicate
template
Provide Feedback