- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Manage data uploaded from a device
Retain or delete data from retentivity storage for a project that was uploaded from a device.
Prerequisites
- Upload a project from device. See Open a project.
- To manage data uploaded from a device
- InProject view, hover over a retentivity storage and select.

- InApply retained data, select either:
- Apply. Apply data retained from the project that was uploaded from the device.
- Delete. Discard data retained from the project that was uploaded from the device.
- Cancel. Cancel the operation.
data
upload
Provide Feedback