- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
HTTP methods
The REST API Client NetLogic exposes these HTTP methods: GET, POST, PUT.
Get
Use the GET method to request data from an API endpoint.
Argument | Description |
---|---|
apiUrl | Address of an endpoint to access the API. |
queryString | Arguments to pass to the API endpoint. |
bearerToken | Token to authenticate the request. |
Post
Use the POST method to send data to an API endpoint and create a resource on the server.
Argument | Description |
---|---|
apiUrl | Address of an endpoint to access the API. |
requestBody | Data to send to the server behind the API endpoint. |
bearerToken | Token to authenticate the request. |
contentType | The original media type of the resource. |
Put
Use the PUT method to send data to an API endpoint and create or replace a resource on the server.
Argument | Description |
---|---|
apiUrl | Address of an endpoint to access the API. |
requestBody | Data to send to the server behind the API endpoint. |
bearerToken | Token to authenticate the request. |
contentType | The original media type of the resource. |
Provide Feedback