- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Third-party .NET libraries
Extend the C# programming language capabilities using third-party .NET libraries.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 8 destination
framework. To debug FactoryTalk Optix Applications
with Visual Studio®
or Visual Studio Code®
, install .NET SDK.Add a third-party library in the editor of your choice. See Add a third-party library to the Visual Studio project and Add a third-party library to the Visual Studio Code project.
Provide Feedback