Development and scripting FAQs

Development and scripting FAQs

How do I develop scripts in FactoryTalk Optix Studio? What languages are supported?
You can develop NetLogic scripts in C# with the use of FactoryTalk Optix Studio and an external code editor to extend the functionalities of your FactoryTalk Optix projects. See Extending projects.
Are there any NetLogic script examples available?
Yes, there are NetLogic script examples. See NetLogic tutorial.
Can I use external packages in my NetLogic scripts?
Yes, you can use external NuGet® packages in your NetLogic scripts. See NuGet packages.
To work with a specific firmware do I have to use a particular FactoryTalk Optix version?
For firmware 6, you must use FactoryTalk Optix version 1.5 or greater.
Can I develop responsive UI with FactoryTalk Optix?
Yes, you can develop responsive UI with FactoryTalk Optix Studio. See Responsive user interface.
Where can I find and download FactoryTalk Optix application examples?
You can find and download FactoryTalk Optix Application examples in the FactoryTalk Optix Help. See Application examples. You can also find examples on the FactoryTalk Hub
Resources
page.
What are the available communication drivers in FactoryTalk Optix?
You can check and learn about the available communication drivers in FactoryTalk Optix Help. See Communication drivers overview and Communication drivers.
Can I downgrade the firmware of an Optix Panel?
No, the only way to downgrade firmware of an Optix Panel is to perform a factory reset of the panel.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.