- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Add users
Add users with different locales.
Prerequisites
Add the it-IT locale. See Add a locale language to a localization dictionary.
- To add users
- InProject view, expandSecurity.
- Create two users by right-clickingUsersand selecting .
- Rename the users by hovering-over each user, selecting, and entering:
- Alice
- Jeremy
- InProject view, selectAlice.
- InProperties, setLocaletoit-IT.
Provide Feedback