Add a panel loader and a NetLogic
Create a panel loader and add the Change Page From Tag NetLogic.
- InProject view, right-clickMainWindow (type)and select .
- From the toolbar, select.Template Libraries
- InLibraries, search forChange Page From Tag
- UnderComponents, dragChange Page From TagtoMainWindow (type).
- InProperties:
- Create a dynamic link betweenPanelLoaderand .
- Create a dynamic link betweenPageChangeTagand .
- Create a dynamic link betweenScreensFolderand .
Provide Feedback