- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a confirmation dialog widget
Add a preconfigured confirmation dialog widget from the template libraries.
- From the toolbar, select.Template Libraries
- InLibraries, search forConfirmation Dialog.
- UnderComponents, dragConfirmation DialogintoUIinProject view.
Provide Feedback