Activate a FactoryTalk Optix Runtime entitlement on Windows devices

Activate a FactoryTalk Optix Runtime entitlement on Windows devices

Activate a Runtime Tools entitlement to launch the application on the Runtime device.
TIP: A runtime device running Windows can have multiple licenses. Each runtime device is associated with one of the available entitlements.
  1. Select the Windows
    Start
    menu and start typing
    Entitlement Manager
    or double-click the
    FactoryTalk® Optix Studio
    icon on your desktop.
  2. In
    Entitlement Manager
    , under
    Installed entitlements
    , select the entitlement type:
    • Online
      : Activate an online entitlement.
    • Offline
      : Activate an offline entitlement.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal