- Software components setup and installation
How to register a router
IMPORTANT:
Follow the instructions below to register your device, based on the device type and its firmware version.
If your device is a
Stratix 4300
, proceed as follows:®
featuring a firmware version older than or equal to 4.0.2- Access the FactoryTalk Remote Access Manager and select.
- Click on thecircled plusicon next to a folder: a context menu will appear.
- Select.NOTE: dialog window appears asking for permission to open the Tool. Prior to confirming, flag theAlways allowcheckbox to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
- Enter the router credentials in the Tool.
- SelectNext.
- TheRouters foundlist displays the MAC addresses of the routers in your domain that have a password matching the one specified.NOTE:When setting up Stratix 4300 Remote Access routers, the username of the router is alwaysadminand cannot be changed. The default password isadminand shall be changed during the initial configuration.You can change the router password anytime through the router System Manager, in theUserssection. Reboot your router upon any password change.Choose a password that contains:
- At least one uppercase character
- At least one lowercase character
- At least one numeric character
- At least one symbol
- Select a router MAC address from the list and clickRegisterto open the configuration pages for that router.NOTE: You might be required to authenticate to theDevice RegistrationTool prior continuing with the router registration.
- The newly connected router appears below the other devices listed in the left pane of.
NOTE:
See Router connection and configuration to configure a router.
If your device is one of the following:
- Stratix 4300®featuring a firmware version newer than 4.0.2
- OptixPanel™featuring a firmware version 4.0.4 or newer
- Embedded Egde Compute Module featuring a firmware version 4.0.4 or newer
proceed as follows:
- Access theFactoryTalk Remote Access Managerand select .
- A dialog box appears. Choose the second choice.NOTE: dialog window appears asking for permission to open the Tool. Prior to confirming, flag theAlways allowcheckbox to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
- A discovery window appears. Click onDiscover.
- TheDiscovered deviceslist displays the devices in your network.
- Select the device that you wish to configure.NOTE:Configurabledevices are still to be initialized on the device System Manager, whileConfigureddevices are already initialized on the device System Manager and the device credentials can be found there.
NOTE:
See Router connection and configuration to configure a router.
Provide Feedback