Top Menu

Top Menu

When you open Twin Studio you are taken to a Quick Access screen with the Twin Studio enabled applications. When you select an application and launch from Quick Access, a tool bar appears across the top of the work space. A menu for Twin Studio access to FactoryTalk Vault appears at the bottom left of the screen.
See Work with FactoryTalk Vault. The other menu options on the screen are application specific to the application you have opened. The following table describes the top menu selections.
FactoryTalk Twin Studio Top Menu Toolbar
Icon
Name
Description
Catalog
View and select applications that are currently available from the Quick Access session you are in. The catalog shows the applications that are installed and available for that particular image in Quick Access. The available applications by Quick Access image are as follows:
In
Emulate3D
:
  • Emulate 3D
  • FactoryTalk Logix Echo
  • FT View ME Station
  • Home Folder
  • Logix Designer
  • View Designer
In
Arena
:
  • Acrobat
  • Arena
  • Excel
  • Home Folder
In
Studio 5000 Logix Designer
:
  • FactoryTalk Logix Echo
  • Logix Designer
Windows
Change between open applications.
My Files
This selection allows access to the files hosted in your Quick Access session. It also allows you to upload files your local computer into the Quick Access session. From here you can select files and
Rename,
Delete,
or 
Download
them. You can create folders and upload files to your system. You can also see basic file information such as date last modified and the size of files. You can also upload files from your computer to the application you are working with.
Clipboard
Allows  you to copy or paste compatible information between your Quick Access session and your local computer desktop.
Microphone
Not applicable to Quick Access - toggle computer microphone on and off.
Camera
Not applicable to Quick Access - toggle computer camera on and off.
Preferences
Customize the resolution, keyboard options, and color interface of your Quick Access session.
FN Keys
Not applicable to Quick Access - opens the list of Windows function keys.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal