Equipment Phase Instructions
The Equipment Phase instructions include:
Available Instructions
Ladder Diagram and Structured Text
Function Block
These instructions are not available in function block.
If want to: | Use this instruction: |
---|---|
Signal an equipment phase that the state routine is complete to indicate that it should go to the next state | PSC |
Change the state or substate of an equipment phase | PCMD |
Give a Hold, Stop, or Abort command to an equipment phase, regardless of ownership | POVR |
Signal a failure for an equipment phase | PFL |
Clear the failure code of an equipment phase | PCLF |
Initiate communication with FactoryTalk Batch software. | PXRQ |
Clear the NewInputParameters bit of an equipment phase | PRNP |
Set up breakpoints within the logic of an equipment phase | PPD |
Take ownership of an equipment phase to either:
| PATT |
Relinquish ownership of an equipment phase | PDET |
Provide Feedback