DCA-DCAF wiring-programming example

This example complies with ISO13849 PLe and IEC61511 SIL 3 operation. It is an example of a relatively simple safety application where temperature sensors are represented by the two 4-wire sensors.
The example shows how to interface the field devices to a 1734-IE4S POINTGuard Analog Input module. The example illustrates how to configure the I/O modules and use I/O tags in the associated logic for this simple application, including how to use the Dual Channel Analog input instruction to control the safety aspects of this application. The standard/control part of this application is not shown.
This example does not include I/O conditioning and fault latching logic, which can be desired for diagnostic reasons.
Wiring Example
DCA_F_wiringexample
(1) Signal Return and Common are at the same potential.
(2) If the sensor has a digital output for use with the Tachometer mode, it must be a push-pull type or have appropriate pull-up or pull-down resistors for NPN or PNP type. The 1734-IE4S module does not provide low impedance of these pull-up or pull-down resistors.
(3) This wiring configuration is also used for SIL 2 redundant Tachometer mode
(4) For analog voltage output sensors, the signal levels for operation for the application must be outside the signal level when the signal is not present, for example, when the wire is broken.
Programming Example
This programming diagram shows the instructions with inputs.
DCA and DCAF programming diagram
Ladder Diagram
DCA_DCAF_other_LD_v31
The programming software is used to configure the input parameters of the Guard I/O module, as illustrated.
Configure the module as shown in the following diagram.
Module Definition
DCA_DCAF_mod definition_v31
Rockwell Automation
suggests selecting
Exact Match
for the
Electronic Keying
as shown. You can also select
Compatible Match
.
Configure the inputs of the module as shown in the following diagrams.
Module Safety Input Configuration
DCA_DCAF_mod safety inp config_v31
Module Input Configuration
DCA_DCAF_Mod_inp_config_v31
Configure Module 1 Alarm Configuration for Channel 0 and 1. Configure channel 0, and then configure Channel 1 identical to Channel 0.
IMPORTANT:
Do not select the Alarm check boxes, because it enables the Analog Modules dual channel feature, which must not be used with the DCA instruction.
Alarm Configuration
DCA_DCAF_alrm config_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.